examples and debugging MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

examples and debugging MQX

ソリューションへジャンプ
1,679件の閲覧回数
Microfelix
Contributor IV

Hi, I recently started working on the K60 and precisely TWRK60-KIT. With the examplesof the K60 I have no problems. Instead if I try to run the examples of the MQX, I can not get it to compile, debug it. I do not know how to run the examples in the folder MQX.Something wrong. Can you help me or point the way to successfully run the examples?

 

thanks Maurizio

0 件の賞賛
返信
1 解決策
1,491件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

I'd recommend going through the Kinetis Quick Start Demo lab, which has detailed instructions for running an MQX project and flashing/debugging it with both CodeWarrior 10 and IAR.

 

You can also look at the docs folder for two files that will also help you get up and going:

\doc\FSL_MQX_3_7_in_CW_10_1.pdf

\doc\FSL_MQX_Getting_Started.pdf

 

Hope that helps!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,492件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

I'd recommend going through the Kinetis Quick Start Demo lab, which has detailed instructions for running an MQX project and flashing/debugging it with both CodeWarrior 10 and IAR.

 

You can also look at the docs folder for two files that will also help you get up and going:

\doc\FSL_MQX_3_7_in_CW_10_1.pdf

\doc\FSL_MQX_Getting_Started.pdf

 

Hope that helps!

0 件の賞賛
返信
1,491件の閲覧回数
Microfelix
Contributor IV

Thank you.

I'm getting closer to Freescale are so many things to see

 

maurizio


0 件の賞賛
返信