example using IO_IOCTL_SERIAL_GET_STATS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

example using IO_IOCTL_SERIAL_GET_STATS

ソリューションへジャンプ
2,926件の閲覧回数
leepenn
Contributor III

Does anyone have an example on using IO_IOCTL_SERIAL_GET_STATS to see the io_info_ptr->RX_CHARS? I am having trouble determining how to properly turn the params pointer into the io_info_ptr.

Thanks,

Lee

0 件の賞賛
返信
1 解決策
2,573件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Lee Penn,

IO_IOCTL_SERIAL_GET_STATS is used to get the statistics information of the serial port, e.g. Rx parity error, overrun, etc.    If you want to check whether there is character received, _io_fstatus() could be used like:        bCharRecved = _io_fstatus(uart3_file);

You may use that code as reference. I hope it helps!!!

Have a great day,

Sol


-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

/* Task IDs */

#define NILL_TASK 5

extern void nill_task(uint_32);

KUART_INFO_STRUCT stats;

// serial port settings

uint_32 baud = 9600, *baud_ptr = &baud;

uint_32 databits = 9, *databits_ptr = &databits;

uint_32 stopbits = 1, *stopbits_ptr = &stopbits;

//uint_8 parity = IO_SERIAL_PARITY_NONE, *parity_ptr = &parity;

uint_32 parity = IO_SERIAL_PARITY_EVEN, *parity_ptr = &parity;

//uint_8 parity = IO_SERIAL_PARITY_ODD, *parity_ptr = &parity;

//uint_8 parity = IO_SERIAL_PARITY_MARK, *parity_ptr = &parity;

const unsigned char serial_options = (IO_SERIAL_RAW_IO);

const char sendstring[] = "ABCDEFGHIJKLMNOPQRSTUVWXYZ0123456789abcdefghijklmnopqrstuvwxyz", *sendstring_ptr = &sendstring[0];

char recvstring[20];

const TASK_TEMPLATE_STRUCT MQX_template_list[] =

{

  /* Task Index, Function, Stack, Priority, Name, Attributes, Param, Time Slice */

  { NILL_TASK, nill_task, 4000, 8, "nill", MQX_AUTO_START_TASK, 0, 0 },

  { 0 }

};

/*TASK*-----------------------------------------------------

*

* Task Name : nill_task

* Comments :

* This task does nothing

*

*END*-----------------------------------------------------*/

void nill_task

  (

  uint_32 initial_data

  )

{

  MQX_FILE_PTR serial_fd;

  uint_32 flags = IO_SERIAL_NON_BLOCKING;

  serial_fd = fopen("ttyd:", (char const*) serial_options);

  ioctl(serial_fd, IO_IOCTL_SERIAL_SET_BAUD, baud_ptr);

  ioctl(serial_fd, IO_IOCTL_SERIAL_SET_FLAGS,&flags );

  write(serial_fd, (void *) sendstring_ptr, 62);

  ioctl( serial_fd , IO_IOCTL_SERIAL_WAIT_FOR_TC, NULL );

  fflush(serial_fd);

  ioctl( serial_fd, IO_IOCTL_SERIAL_GET_STATS, (pointer)&stats);

  ioctl(serial_fd, IO_IOCTL_SERIAL_GET_FLAGS,&flags );

  while(1)

  read(serial_fd, recvstring, 20);

  _io_fclose(serial_fd);

  _mqx_exit(0);

}

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,573件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Lee,

I have implemented it in the code at the following post differently than soledad (her approach is nicer):

Receiving characters from a UART under MQX

I was looking at the  RX_OVERRUNS field specifically buy with the call below you get all the flags to review.

  uint32_t param[15];          //DES has extra room to buffer

      if(lengthRead) {

        _io_ioctl(stdout, IO_IOCTL_SERIAL_GET_STATS, &param);          //DES get UART statisics

        if(param[7]) {          //DES check RX_OVERRUNS

          _io_puts("\nRX_OVERRUNS Error...\n");

          fflush(stdout);

          _io_ioctl(stdout, IO_IOCTL_SERIAL_CLEAR_STATS, &param);          //DES clear UART statisics

        }

Look in serl_kuart.h for definitions of the Stats.

typedef struct kuart_info_struct

{

   /* The current init values for this port */

   KUART_INIT_STRUCT          INIT;

   /* The sci device register */

   UART_MemMapPtr             SCI_PTR;

   /* The previous interrupt handler and data */

   void       (_CODE_PTR_ OLD_ISR)(void *);

   void       (_CODE_PTR_ OLD_ISR_EXCEPTION_HANDLER)(uint32_t, uint32_t, void *,

               void *);

   void                             *OLD_ISR_DATA;

   /* Various flags */

   uint32_t                           FLAGS;

  

   /* Statistical information */

   uint32_t                           INTERRUPTS;

   uint32_t                           RX_CHARS;

   uint32_t                           TX_CHARS;

   uint32_t                           RX_BREAKS;

   uint32_t                           RX_PARITY_ERRORS;

   uint32_t                           RX_FRAMING_ERRORS;

   uint32_t                           RX_OVERRUNS;

   uint32_t                           RX_DROPPED_INPUT;

   uint32_t                           RX_NOISE_ERRORS;

Look in serl_pol_kuart.c for the order in which the param array gets filled as it is slightly different than the definition order.

      case IO_IOCTL_SERIAL_GET_STATS:

         *param_ptr++ = io_info_ptr->INTERRUPTS;

         *param_ptr++ = io_info_ptr->RX_CHARS;

         *param_ptr++ = io_info_ptr->TX_CHARS;

         *param_ptr++ = io_info_ptr->RX_BREAKS;

         *param_ptr++ = io_info_ptr->RX_PARITY_ERRORS;

         *param_ptr++ = io_info_ptr->RX_FRAMING_ERRORS;

         *param_ptr++ = io_info_ptr->RX_OVERRUNS;

         *param_ptr++ = io_info_ptr->RX_DROPPED_INPUT;

         *param_ptr++ = io_info_ptr->RX_NOISE_ERRORS;

         break;

Regards,

David

2,574件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Lee Penn,

IO_IOCTL_SERIAL_GET_STATS is used to get the statistics information of the serial port, e.g. Rx parity error, overrun, etc.    If you want to check whether there is character received, _io_fstatus() could be used like:        bCharRecved = _io_fstatus(uart3_file);

You may use that code as reference. I hope it helps!!!

Have a great day,

Sol


-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

/* Task IDs */

#define NILL_TASK 5

extern void nill_task(uint_32);

KUART_INFO_STRUCT stats;

// serial port settings

uint_32 baud = 9600, *baud_ptr = &baud;

uint_32 databits = 9, *databits_ptr = &databits;

uint_32 stopbits = 1, *stopbits_ptr = &stopbits;

//uint_8 parity = IO_SERIAL_PARITY_NONE, *parity_ptr = &parity;

uint_32 parity = IO_SERIAL_PARITY_EVEN, *parity_ptr = &parity;

//uint_8 parity = IO_SERIAL_PARITY_ODD, *parity_ptr = &parity;

//uint_8 parity = IO_SERIAL_PARITY_MARK, *parity_ptr = &parity;

const unsigned char serial_options = (IO_SERIAL_RAW_IO);

const char sendstring[] = "ABCDEFGHIJKLMNOPQRSTUVWXYZ0123456789abcdefghijklmnopqrstuvwxyz", *sendstring_ptr = &sendstring[0];

char recvstring[20];

const TASK_TEMPLATE_STRUCT MQX_template_list[] =

{

  /* Task Index, Function, Stack, Priority, Name, Attributes, Param, Time Slice */

  { NILL_TASK, nill_task, 4000, 8, "nill", MQX_AUTO_START_TASK, 0, 0 },

  { 0 }

};

/*TASK*-----------------------------------------------------

*

* Task Name : nill_task

* Comments :

* This task does nothing

*

*END*-----------------------------------------------------*/

void nill_task

  (

  uint_32 initial_data

  )

{

  MQX_FILE_PTR serial_fd;

  uint_32 flags = IO_SERIAL_NON_BLOCKING;

  serial_fd = fopen("ttyd:", (char const*) serial_options);

  ioctl(serial_fd, IO_IOCTL_SERIAL_SET_BAUD, baud_ptr);

  ioctl(serial_fd, IO_IOCTL_SERIAL_SET_FLAGS,&flags );

  write(serial_fd, (void *) sendstring_ptr, 62);

  ioctl( serial_fd , IO_IOCTL_SERIAL_WAIT_FOR_TC, NULL );

  fflush(serial_fd);

  ioctl( serial_fd, IO_IOCTL_SERIAL_GET_STATS, (pointer)&stats);

  ioctl(serial_fd, IO_IOCTL_SERIAL_GET_FLAGS,&flags );

  while(1)

  read(serial_fd, recvstring, 20);

  _io_fclose(serial_fd);

  _mqx_exit(0);

}

0 件の賞賛
返信