eGui using D4D_menu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eGui using D4D_menu

1,350件の閲覧回数
av-icode
Contributor I

Hi

I'm trying to use D4D_Menu, according to the example in: d4d_screen_winmenu.c

The D4D_Menu is fine when the position is: x=0,y=0.

The problem when I define D4D_Menu with position: X=50, y=50, the position of the scroll bar is not aligned with the list box.

I'm using K70 tower and egui/d4d version3.

==============================================================================

D4D_Menu is fine when the position is: x=0,y=0.

20150531_122806_t.jpg

=================================================================================

D4D_Menu with position: X=50, y=50, scroll bar with offset

20150531_123032_t.jpg

=================================================================================

I add fix in Git Hub:

pastedImage_0.png

タグ(2)
0 件の賞賛
返信
1 返信

1,200件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello joni?

Have you solved your problem?

Regards


Soledad

0 件の賞賛
返信