cw 10.2 and MQX 3.8 install issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cw 10.2 and MQX 3.8 install issue

ソリューションへジャンプ
1,412件の閲覧回数
barbercolman
Contributor III

I installed CW 10.2 then installed MQX 3.8 and then tried to install TAD and plugging. I received the an error "The copies of profile PlatformProfile are not in sync". How do I find there issues? Interesting note the log file can not found

 

Any help?

 

 

The following is a copy of the cmd window  i was using to install.
c:\Freescale\Freescale MQX 3.8\tools\codewarrior_extensions\CW MCU v10.2>install
_cw10.2_plugin.bat "c:\freescale\cw mcu v10.2"
 **** Installing CW10.2 Task Aware Debugging and New Project Wizard Plugins ***
 **** It can take up to 60 seconds ***
**** Installing plug-ins for MQX 3.8 ****
Installing com.freescale.mqx.v3.8.feature.group 1.1.0.201112071639.
Operation completed in 7388 ms.
**** Installing plug-ins for MQX - all versions ****
Installing com.freescale.mqx.common.feature.group 1.1.0.201112071639.
Installation failed.
The copies of profile PlatformProfile are not in sync.
Application failed, log file location: C:\Freescale\CW MCU v10.2\eclipse\configu
ration\1338491104240.log
 **** Installing CW10.2 Processor Expert MQX RTOS Adapter update ****
17 File(s) copied
 **** Done ****

c:\Freescale\Freescale MQX 3.8\tools\codewarrior_extensions\CW MCU v10.2>bat "c:\Freescale\CW MCU v10.2

0 件の賞賛
返信
1 解決策
994件の閲覧回数
MarcinG
Contributor III

This problem might be similar to this one: https://community.freescale.com/thread/109684 

 

Try to use updated scripts, hopefully it will help. You may find them attached to the mentioned thread or at the Freescale website: MQX_3.8_INST_CW_MCU_10.2_UP_v1.0.0_SP.zip

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
995件の閲覧回数
MarcinG
Contributor III

This problem might be similar to this one: https://community.freescale.com/thread/109684 

 

Try to use updated scripts, hopefully it will help. You may find them attached to the mentioned thread or at the Freescale website: MQX_3.8_INST_CW_MCU_10.2_UP_v1.0.0_SP.zip

 

 

0 件の賞賛
返信
994件の閲覧回数
barbercolman
Contributor III

Thank you it worked.

 

On a related topic. Does any on know when the "default directory" will be updated from "c:\program files..."?

0 件の賞賛
返信