cdc virtual_com example not working on Kwikstik

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cdc virtual_com example not working on Kwikstik

ソリューションへジャンプ
3,053件の閲覧回数
mpc8377e
Contributor I

Hi,

 

I am trying to run CDC virtual_com example on K40 Kwikstik board. I can send data from host (windows xp) to device and can print the data received but the data sent from device is not received by the host. 

 

The same example works fine on k40 Towermoulde.

 

Any solutions for this problem.

 

Regards,

Raghu

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,682件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

good news: my problem has been solved with the attached .inf file :smileyhappy:.

 

BK

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,682件の閲覧回数
c0170
Senior Contributor III

Hi mpc8377e,

 

does your problem persist or any progress made? I'll test that example and get back to you with the result.

 

Regards,

MartinK

0 件の賞賛
返信
2,682件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi there,

for information: I have the same problem: I can send data from the host to the KwikStik, but cannot send from the KwikStik to the host:

https://community.freescale.com/message/112100#112100

 

BK

0 件の賞賛
返信
2,683件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

good news: my problem has been solved with the attached .inf file :smileyhappy:.

 

BK

0 件の賞賛
返信
2,682件の閲覧回数
MarkP_
Contributor V

Hi,

same problem with MQX4.0 and CW10.4.

Does that inf-file change fix it?

Where can I get it?

~Mark

0 件の賞賛
返信