can we write cpp code using codewarrior Version: 10.4 and mqx 4.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can we write cpp code using codewarrior Version: 10.4 and mqx 4.0

1,211 Views
josephxavier
Contributor III

can we write cpp code using codewarrior Version: 10.4 and  mqx 4.0, what are the steps to do so?

0 Kudos
Reply
1 Reply

1,132 Views
soledad
NXP Employee
NXP Employee

Hello Jose,

Yes, in addition you can use as reference the example code located at the path: C:\Freescale\Freescale_MQX_4_0\mqx\examples\cplus\cw10

I hope this helps!!


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply