bug in MQX getaddrinfo() with IPv6 enabled?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bug in MQX getaddrinfo() with IPv6 enabled?

2,102件の閲覧回数
m_bach
Contributor III

Hi Community,

 

I using MQX with IPv6, so enabled RTCSCFG_ENABLE_IP6

 

Now when I'm using get getaddrinfo() with an FQDN, getaddrinfo() always fails if my DNS Server does not reply AAAA queries...

 

Whats happening:

- getaddrinfo() sends the 'A' record query to my DNS server, and collects the qualified answer. Everything is fine.

- next in line due to NET_ORDER is the INET6 family query

- getaddrinfo() then sends a subsequent 'AAAA' query, which is not fully responded by my DNS Server for this host.

- then getaddrinfo() returns error(4), which is odd because the 'A' record was replied fine.

 

I patched getaddrinfo.c accoringly, and want to know what you think about this.

 

cheers, Martin

Original Attachment has been moved to: getaddrinfo.c.patch.zip

0 件の賞賛
返信
5 返答(返信)

1,865件の閲覧回数
RadekS
NXP Employee
NXP Employee

It is known issue. It was already fixed on development branch.

In attachment you can find latest version of getaddrinfo.c file.


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,865件の閲覧回数
m_bach
Contributor III

sorry, can't compile....

(Y:\MQX\rtcs\source\if\getaddrinfo.c|640|59|1|19503|1)

=        if((ip_addr = RTCS_hosts_get_addr(hostname, family)) != NULL) 

>illegal implicit conversion from 'int' to

>'void *'

(Y:\MQX\rtcs\source\if\getaddrinfo.c|674|64|1|20598|1)

=e, '.') == NULL) && ((dns_suffix = RTCS_get_primary_dns_suffix()) != NULL )) 

>illegal implicit conversion from 'int' to

>'const char *'

(Y:\\MQX\rtcs\source\if\getaddrinfo.c|700|53|1|21815|1)

=                dns_params.name_to_resolve = hostname;      /* Host name to resolve (null-terminated string). */              

>illegal implicit conversion from 'const char *' to

>'char *'

seems I'm lacking some new function defs, such as RTCS_hosts_get_addr()  and RTCS_get_primary_dns_suffix() ...

0 件の賞賛
返信

1,865件の閲覧回数
m_bach
Contributor III

Hi RadekS, thanks a lot!

I'm just checking your changes. Which is a little hard, because there is a change in tabs/spaces style. I have to ignore whitespace changes ...

Is there a way to follow the MQX developpent branch? Any public source code repository available?

thanks, Martin

0 件の賞賛
返信

1,865件の閲覧回数
RadekS
NXP Employee
NXP Employee

No, unfortunately currently it is not possible. MQX is released only in periodic intervals.

You are right, attached getaddrinfo.c contains more changes and some of these changes don’t need be anyway connected to this bug. It is just snippet from current source code.

You should take it only as inspiration…

1,865件の閲覧回数
m_bach
Contributor III

ok, you got it :smileywink:

0 件の賞賛
返信