booting MQX from an SD Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

booting MQX from an SD Card

2,050件の閲覧回数
MKnecht
Contributor I

Hi,

 

is it possible / are there BSP that support MQX alternatively booting

from an SD Card ?

 

regards

 

Michael

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,337件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Michael,

Currently no bootling from SD card.

On our MCF54418 family we can boot from NAND flash.

If you are using a microprocessor with enough memory resources, you can create a FSLMQX image to be a SD Card bootloader that will erase and re-program your FSLMQX application.

Regards,

David

0 件の賞賛
返信

1,338件の閲覧回数
MKnecht
Contributor I

Hi David,

 

is there any example code / project for this purpose?

SW update via SD Card is often announced in the Freescale kinetis leaflets.

So there should already be an out of the box solution.

 

regards

 

Michael

0 件の賞賛
返信