booting MQX from an SD Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

booting MQX from an SD Card

1,064 Views
MKnecht
Contributor I

Hi,

 

is it possible / are there BSP that support MQX alternatively booting

from an SD Card ?

 

regards

 

Michael

Tags (2)
0 Kudos
2 Replies

351 Views
DavidS
NXP Employee
NXP Employee

Hi Michael,

Currently no bootling from SD card.

On our MCF54418 family we can boot from NAND flash.

If you are using a microprocessor with enough memory resources, you can create a FSLMQX image to be a SD Card bootloader that will erase and re-program your FSLMQX application.

Regards,

David

0 Kudos

351 Views
MKnecht
Contributor I

Hi David,

 

is there any example code / project for this purpose?

SW update via SD Card is often announced in the Freescale kinetis leaflets.

So there should already be an out of the box solution.

 

regards

 

Michael

0 Kudos