bitbake -DDD fsl-image-qt5-validation-imx -c populate_sdk 4.14.98 fails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bitbake -DDD fsl-image-qt5-validation-imx -c populate_sdk 4.14.98 fails

1,507件の閲覧回数
terry1
Contributor III

bitbake -DDD fsl-image-qt5-validation-imx -c populate_sdk

This fails, and why is there an x86_64-deploy_fsl-image-qt5-validation-imx-populate-sdk, for an imx8?

ERROR: fsl-image-qt5-validation-imx-1.0-r0 do_populate_sdk: Build of do_populate_sdk failed
ERROR: fsl-image-qt5-validation-imx-1.0-r0 do_populate_sdk: Traceback (most recent call last):
File "/home/imx8/imx-yocto-bsp/sources/poky/bitbake/lib/bb/build.py", line 644, in exec_task
return _exec_task(fn, task, d, quieterr)
File "/home/imx8/imx-yocto-bsp/sources/poky/bitbake/lib/bb/build.py", line 582, in _exec_task
exec_func(task, localdata)
File "/home/imx8/imx-yocto-bsp/sources/poky/bitbake/lib/bb/build.py", line 202, in exec_func
bb.utils.mkdirhier(cdir)
File "/home/imx8/imx-yocto-bsp/sources/poky/bitbake/lib/bb/utils.py", line 734, in mkdirhier
raise e
File "/home/imx8/imx-yocto-bsp/sources/poky/bitbake/lib/bb/utils.py", line 731, in mkdirhier
os.makedirs(directory)
File "/usr/lib/python3.6/os.py", line 220, in makedirs
mkdir(name, mode)
PermissionError: [Errno 13] Permission denied: '/home/imx8/imx-yocto-bsp/build-xwayland/tmp/work/imx8mqevk-poky-linux/fsl-image-qt5-validation-imx/1.0-r0/x86_64-deploy-fsl-image-qt5-validation-imx-populate-sdk'

ERROR: Task (/home/imx8/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/dynamic-layers/qt5-layer/recipes-fsl/images/fsl-image-qt5-validation-imx.bb:do_populate_sdk) failed with exit code '1'
DEBUG: Teardown for bitbake-worker
DEBUG: Teardown for bitbake-worker
NOTE: Tasks Summary: Attempted 7809 tasks of which 7808 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/imx8/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/dynamic-layers/qt5-layer/recipes-fsl/images/fsl-image-qt5-validation-imx.bb:do_populate_sdk
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

0 件の賞賛
返信
1 返信

1,303件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Are you using ubuntu? seems there is "permission" issue of the folder in your linux host.

0 件の賞賛
返信