Working sets (MQX-specific)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Working sets (MQX-specific)

ソリューションへジャンプ
1,804件の閲覧回数
davidsherman
Senior Contributor I

I'm making a new MQX BSP for a K10.  One thing I'm a little confused on is the directory structure.  I had previously used the twr-k20d50m board and had MQX running on it.  If I import the working set for one of the examples for the twr-k20d50m, I see the BSP, PSP, and application trees.  If I look at the properties for the directories and files within them, I see directories for the peripheral drivers such as:

/bsp_twrk20d50m/Peripheral_IO_Drivers/

I can see that same directory in:

C:\Freescale\Freescale_MQX_4_2\mqx\build\kds\bsp_twrk20d50m

However, the contents of Peripheral_IO_Drivers is empty in that exact location.

It appears that the contents are actually being referenced in:

C:\Freescale\Freescale_MQX_4_2\mqx\source

Interestingly, KDS seems to show that they are actually in the bsp build directory.

So, am I correct that it's actually referencing directories in the MQX source directory?

That leads to my next question, my new BSP is based on the K60.  The BSP porting tool made a new one alright, but it includes build directories for ethernet and USB, which don't apply to the K10.  I'm assuming that these can be removed from the project to ignore them (I've already excluded them in the build) without affecting the contents of the MQX source directory.

0 件の賞賛
返信
1 解決策
1,635件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello David,

Yes, both assumptions are correct.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,636件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello David,

Yes, both assumptions are correct.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,635件の閲覧回数
davidsherman
Senior Contributor I

Thank you!

0 件の賞賛
返信