Why would USB_Class_CDC_Send_Data not cause a USB_APP_SEND_COMPLETE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why would USB_Class_CDC_Send_Data not cause a USB_APP_SEND_COMPLETE

1,505 Views
pbarada
Contributor II

Using in MQX-4.2.0.2 on a twrk70f120m with a TWR_SER2 we're trying to send a bunch of data over USB CDC and we see that USB transmit/receive are working fine for a while (i.e. multiple minutes) and then things stop after a successful call to USB_CLass_CDC_Send_Data with no following USB_APP_SEND_COMPLETE notify event.

1) Have people seen the MQX EHCI device stack/driver exhibit this behavior?

2) What possible recovery methods could I try?

Thanks in advance!

Labels (1)
0 Kudos
Reply
1 Reply

1,214 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the following threads and let me know if this helps!!
USB CDC on TWR-K60F120M and TWR-SER2 Board won't send certain values. 

https://community.nxp.com/thread/312262#350162 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply