Why does RTCS use rtcs_fd_set for sets of file descriptors instead of just an fd array pointer and count? What are the implications of changing RTCSCFG_FD_SETSIZE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why does RTCS use rtcs_fd_set for sets of file descriptors instead of just an fd array pointer and count? What are the implications of changing RTCSCFG_FD_SETSIZE?

1,105 Views
dmitriyc
Contributor III

Hello,

I am looking at the RTCS manual, specifically the select() function, and wondering why it takes rtcs_fd_set pointers instead of just taking arrays of file descriptors and their respective lengths. Is there some reasoning behind this?

On the one hand, it is somewhat inefficient because the user is forced to use the biggest array ever used in one of these fd_set structures. On the other hand, it leaves room for a dangerous configuration change by making RTCSCFG_FD_SETSIZE configurable in user_config.h. If I change it to, say, 4 from the default 8, everything that uses rtcs_fd_set is at risk of not having a big enough FD set array to operate properly (not to mention possible overruns in unsafe code).

Am I missing something? I'm sure there's a good reason for this design decision, but I can't quite figure out what it is. If a Freescale employee who dealt with that part of the code would explain the reasoning behind it, that would be ideal, but I would also appreciate any speculation on why it's done this way or relevant historical background from other similar APIs.

As a safeguard, I do something similar to

#if RTCSCFG_FD_SETSIZE < 5

#error "RTCS FD SET SIZE TOO SMALL"

#endif

in code that requires a certain FD set size to function. Of course there's also the ability to calculate constants and loop counts based on RTCSCFG_FD_SETSIZE to make things more generic, so the fact that it's changeable really isn't a big deal if the code handles it properly. Mostly, the thing that puzzles me here is the willingness to potentially waste some RAM in an embedded system for the sake of having fewer arguments in API function calls...

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

974 Views
dmitriyc
Contributor III

Partially answering my own question after some more research, it's may be because that's the way POSIX does it. For example, the Linux select manpages: select(2) - Linux manual page  and  fd_set(3): synchronous I/O multiplexing - Linux man page ​.  This makes sense because MQX tries to follow POSIX were possible, but the POSIX API was probably designed primarily for application-level OSes, which would have no problem with an fd_set size of 1024. Would still appreciate some comments from other people on this.

0 Kudos
Reply