Where is the chat_client run.html from MQX + KSDK example?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the chat_client run.html from MQX + KSDK example?

ソリューションへジャンプ
1,865件の閲覧回数
lfschrickte
Contributor IV

Hi,

The updated httpsrv demo for MQX RTOS + KSDK shows an application to the new Web Socket feature and that is cool!

However, the readme file and the own http server asks the user to open a file called run.html on the chat_client folder, but neither of them is available in my files!

I also want to note that in this demo I needed to put lines to init the hardware and serial console in order to put printf to work. I've added both "hardware_init();" and "dbg_uart_init();" calls. I also had to add some files to the compilation, following the lwip examples, from /httpsrv_frdmk64f120m/utilities folder (also added "${ProjDirPath}/../../../../../../../platform/drivers/uart/common/" to the compiler includes). Is there any other right/official way to make this work?

Thank you very much!

Luiz Fernando

ラベル(1)
0 件の賞賛
返信
1 解決策
1,720件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Find attached the file.

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,721件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Find attached the file.

Luis

0 件の賞賛
返信