Where is MQX TWR-WIFI-AR4100 Code ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is MQX TWR-WIFI-AR4100 Code ?

ソリューションへジャンプ
1,503件の閲覧回数
ChrisNielsen
Contributor III


I have MQX 4.0 and I've read the posts on this subject that identifies the \source\io\enet directory as containing AR4100 code.  My download of MQX 4.0 does not have that code.

Does MQX 4.0 support TWR-WIFI-AR4100 or must I move back to an older version that has support?  If support was dropped in the current release, can you share the reason why?  I was hoping to design in the AR4100 part but if it is not longer "recommended for new designs", I'd like to know that quickly.

Are other community members using the AR4100 part or has the community moved to other WiFi parts?

I'm not planning to use MQX.  I just need to get to the MQX driver source code so I can have a working example of SPI and API code that interfaces with the AR4100 chip and I will build upon that code to develop my end system.

Thanks, Chris

0 件の賞賛
返信
1 解決策
1,257件の閲覧回数
Martin_
NXP Employee
NXP Employee

check

https://community.freescale.com/message/318565#318565

In short, download and install the patch for MQX 3.7. There you will get the files that don't install with MQX 4.0 by default.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,258件の閲覧回数
Martin_
NXP Employee
NXP Employee

check

https://community.freescale.com/message/318565#318565

In short, download and install the patch for MQX 3.7. There you will get the files that don't install with MQX 4.0 by default.

0 件の賞賛
返信