Virtual ethernet interface in MQX.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Virtual ethernet interface in MQX.

跳至解决方案
1,421 次查看
namile
Contributor II

I am using MQX 3.8 with Kinetis K60. I need to create a virtual ethernet interface. Is there a way to do that in MQX?

标签 (1)
标记 (5)
0 项奖励
回复
1 解答
1,191 次查看
DavidS
NXP Employee
NXP Employee

Hi Rajesh,

I do not know of TAP being implemented with MQX or even on its roadmap.  I will pass along this request as it is our customer desires that help shape MQX for the future.

From TUN/TAP Driver Info

I see that it is ported to Linux/Solaris/BSD.

Regards,

David

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,191 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Rajesh Namile

Do you mean 802.1q support? Full VLAN support is not implemented in current MQX version. Freescale development team are working on this feature. It will be available with next MQX release. Sorry for the inconvenience that caused


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,191 次查看
namile
Contributor II

I am trying to create a TAP interface for my application.

0 项奖励
回复
1,192 次查看
DavidS
NXP Employee
NXP Employee

Hi Rajesh,

I do not know of TAP being implemented with MQX or even on its roadmap.  I will pass along this request as it is our customer desires that help shape MQX for the future.

From TUN/TAP Driver Info

I see that it is ported to Linux/Solaris/BSD.

Regards,

David

0 项奖励
回复