Virtual ethernet interface in MQX.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Virtual ethernet interface in MQX.

ソリューションへジャンプ
2,539件の閲覧回数
namile
Contributor II

I am using MQX 3.8 with Kinetis K60. I need to create a virtual ethernet interface. Is there a way to do that in MQX?

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
2,309件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Rajesh,

I do not know of TAP being implemented with MQX or even on its roadmap.  I will pass along this request as it is our customer desires that help shape MQX for the future.

From TUN/TAP Driver Info

I see that it is ported to Linux/Solaris/BSD.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,309件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Rajesh Namile

Do you mean 802.1q support? Full VLAN support is not implemented in current MQX version. Freescale development team are working on this feature. It will be available with next MQX release. Sorry for the inconvenience that caused


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,309件の閲覧回数
namile
Contributor II

I am trying to create a TAP interface for my application.

0 件の賞賛
返信
2,310件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Rajesh,

I do not know of TAP being implemented with MQX or even on its roadmap.  I will pass along this request as it is our customer desires that help shape MQX for the future.

From TUN/TAP Driver Info

I see that it is ported to Linux/Solaris/BSD.

Regards,

David

0 件の賞賛
返信