Using PEx in the BSP for KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using PEx in the BSP for KDS

1,076 次查看
Vagni
Contributor IV

In MQX 4.1.1 the pe_demo project is provided also for KDS build configuration, but no PEx project is present in the KDS build configuration for the BSP library (the PEx project for BSP is present only in CW build configuration).

The MQX_BSP_Porting_Example_User_Guide document describes how to set up BSP for PEx with IAR or KEIL build environment.

What about KDS? How can I set up BSP for PEx in KDS build environment? Is there a setup procedure as for IAR and KEIL?

The pe_demo application needs a PEx-based BSP to run...

标记 (4)
0 项奖励
回复
1 回复

812 次查看
soledad
NXP Employee
NXP Employee

Hi Alessandr,

Please check the following thread: MQX + PE for SDK cannot be build with default language standard in KDS toolchain

In addition, please check the below threads,

KDS 1.1.0 adding MQX component using processor expert fails build

MQX with KSDK and Processor Expert


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复