Urgent help needed for eGUI for MCF52277CPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Urgent help needed for eGUI for MCF52277CPU

Jump to solution
1,987 Views
Satya251
Contributor I

Hi ,

  I would like to know following details about eGUI.

1. Can we make PC based(VC++) project for the eGUI?

2.I can only see only few resources are available for eGUI like 

 

 

Button

Check box/user handled radio button

Gauge

Icon

Label

Menu

Picture

Slider

Graph

If more resources are need then what we need to do?

3.Where can I get the demo version of eGUI. If anyone has the link kindly provide it.

Thanks & Regards,

Satyajit

0 Kudos
Reply
1 Solution
1,636 Views
bluehacker
Contributor III

1. it seems not support vc project now, then I think it is no need for this

2. eGUI is just a simple GUI, don't count on very complex and falring display

3. eGUI is completely free, you can download from http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=EGUI&parentCode=MCF5227X&fpsp=1

View solution in original post

0 Kudos
Reply
1 Reply
1,637 Views
bluehacker
Contributor III

1. it seems not support vc project now, then I think it is no need for this

2. eGUI is just a simple GUI, don't count on very complex and falring display

3. eGUI is completely free, you can download from http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=EGUI&parentCode=MCF5227X&fpsp=1

0 Kudos
Reply