USB without MFS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,694件の閲覧回数
Dougdjl
Contributor I

We are using MQX 3.6.1 with a 52259 micro. I'd like to be able to access a USB stick that contains a file loaded from a PC. Is this possible to do without the use of MFS? We're having memory issues. Even though the system has external ram we're having compiler conflicts with MFS/USB and extended memory operation. The difference between light weight memory and not.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,501件の閲覧回数
DavidS
NXP Employee
NXP Employee

The short answer is you need MFS to read a MFS formatted USB drive/stick.

Regards,

David


元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,502件の閲覧回数
DavidS
NXP Employee
NXP Employee

The short answer is you need MFS to read a MFS formatted USB drive/stick.

Regards,

David


0 件の賞賛
返信
1,501件の閲覧回数
Monica
Senior Contributor III

Hey there Douglas!

Any updates on the project?

Sorry for the delay, we'll be shortly working on your issue if there are still memory flaws!

Regards!

Monica

0 件の賞賛
返信