USB without MFS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB without MFS

Jump to solution
1,752 Views
Dougdjl
Contributor I

We are using MQX 3.6.1 with a 52259 micro. I'd like to be able to access a USB stick that contains a file loaded from a PC. Is this possible to do without the use of MFS? We're having memory issues. Even though the system has external ram we're having compiler conflicts with MFS/USB and extended memory operation. The difference between light weight memory and not.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,559 Views
DavidS
NXP Employee
NXP Employee

The short answer is you need MFS to read a MFS formatted USB drive/stick.

Regards,

David


View solution in original post

0 Kudos
Reply
2 Replies
1,560 Views
DavidS
NXP Employee
NXP Employee

The short answer is you need MFS to read a MFS formatted USB drive/stick.

Regards,

David


0 Kudos
Reply
1,559 Views
Monica
Senior Contributor III

Hey there Douglas!

Any updates on the project?

Sorry for the delay, we'll be shortly working on your issue if there are still memory flaws!

Regards!

Monica

0 Kudos
Reply