USB_v2 Error K64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB_v2 Error K64

2,679件の閲覧回数
Microfelix
Contributor IV

Hello,

I compiled the project "host_msd_fatfs_twrk64f120m"

MQX 4.2

KDS 3.0

After compiling libraries and related project, I get an error on the shell closing Filesystem.

Library:

bsp.a

psp.a

shell.a

msf.a

libusbh_mqx.a

can you help me?

error_usb_v2.png

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,413件の閲覧回数
Microfelix
Contributor IV

up

0 件の賞賛
返信

2,413件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Maurizio,

Unfortunately I cannot to reproduce your issue. If you are using the Twr-k64f12m board please check the jumper configurations.

• For USB Host mode, use onboard J17 Micro USB connector and jumpers set to default settings. Connect the J2 (K20

DEBUG) Mini USB to the PC to enable power for the USB Host.

In addition please confirm that the ID pin is grounded.

The ID pin is for detecting if the USB port is Host or Device. When a port is Host, the ID pin should be grounded. If the port is Device, the ID pin should remain floating.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,413件の閲覧回数
Microfelix
Contributor IV

Thanks for the reply.

I am not using the TWR.

I'm using "MK64FN1M0VLL12" smaller  (only 100 pins)

For example, the pin PTE12, pin ID, does not exist.

This problem I had not before using MQX 4.1 and CodeWarrior.

But now using KDS, with USB_v2, I have this problem.

There are settings to change the library USBH?

Thank you.

0 件の賞賛
返信