USB packet not sent if size equal to buffer size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB packet not sent if size equal to buffer size

2,442件の閲覧回数
freuz
Contributor II

Hi all,

I'm using KM20DN512 in USB slave device connected to a windows PC with winUSB driver.

I use the original MQX 4.0 usb device driver with endpoint buffer size to 64bytes in BULK. In according to CDC example demo, I send a zero lenght packet if the modulo of data size to send is equal to endpoint buffer size (data size % 64 == 0). But my problem is if the data size to send is exactly equal to endpoint buffer size, the data packet is not sent (I see no data transaction with the USB sniffer ie TotalPhase Beagle) and I only see the zero lenght packet. In other words, the data packet is sent if size >64 or size<64, not sent if size==64. I have already read and post on this thread with no satisfying answer: https://community.freescale.com/message/304117#304117

Someone have any idea to finally solve this issue?

Thanks!

Frédéric Parent

ラベル(1)
2 返答(返信)

2,066件の閲覧回数
freuz
Contributor II

Can anyone help me in this issue ?

0 件の賞賛
返信

2,066件の閲覧回数
freuz
Contributor II

Finally, I found the problem... with WinUSB.