USB Host Printer Class

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Host Printer Class

6,383件の閲覧回数
Nouchi
Senior Contributor II

Hello,

 

I'm looking for some USB Host Class Printer application exemple.

Where can I find such project?

 

Emmanuel

 

ラベル(1)
タグ(1)
7 返答(返信)

3,733件の閲覧回数
JuroV
NXP Employee
NXP Employee

USB printer class is not supported yet in MQX.

0 件の賞賛
返信

3,733件の閲覧回数
Nouchi
Senior Contributor II

Hello,

 

It was added in MQX 3.5, it's written in release notes :

 

 

4.5.1 USB Class Drivers supported by Host Development Kit- Human-interface Class (HID) used to access mouse, keyboard and similar devices.- Mass storage device (MSD) Class used to access USB drives.- USB Hub class used to attach multiple devices to a single host port. If enabled at theapplication level, the HUB support is fully transparent. User application only needs to bemodified to be ready to handle multiple USB devices simultaneously. Keyboard/Mouseexample application is provided.- Basic Printer class.

 

 

 

0 件の賞賛
返信

3,733件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hello,

 

I am sorry to say that, but printer class is really not supported in MQX, even not in MQX 3.5.

0 件の賞賛
返信

3,733件の閲覧回数
evgenyerlihman
Contributor IV

Hi JuroV​,

Do you know if MQX4.2 support usb printer?

Thanks,

Evgeny

0 件の賞賛
返信

3,733件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Evgeny,

The MQX 4.x support the USB host printer class and you can find the driver from: .../usb/host/source/classes/printer.

Unfortunately we don't have any source code example for using that class driver, (we've not tested it) and so we can hardly estimate the effort.

Theoretically, to communicate with the printer should be easy (enumerate, interface, send bulk data) as these functions are prepared in the class driver. The printer language needs to be implemented at the application level. Unfortunately we don't have experience with it that we could share at the moment.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,732件の閲覧回数
Nouchi
Senior Contributor II

Hello,

 

I'm little bit obstinate and impatient, I guess it's a feature for future release.

But, you can find files named usb_host_printer.c and usb_host_printer.h, holding functions like usb_printer_init, usb_printer_recv_data, usb_printer_send_data and some other.

Interesting, no ?

 

 

0 件の賞賛
返信

3,733件の閲覧回数
nikhil165
Contributor I

Does MQX 3.8 supports printer class?

0 件の賞賛
返信