USB File Read Speed with MQX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB File Read Speed with MQX

Jump to solution
2,387 Views
amish_M4
Contributor I

We are using MQX 3.8 on a K70, internal USB Full Speed.  The K70 is set as the Host and reading a file from a USB Flash Drive using the MQX MFS File System. The file is a binary file about 2MB in size.  It takes 7-8 seconds on a few drives to load the file, but on most drives it takes 40-60 seconds. This seems really slow for a Full Speed USB connection..?

 

 

 

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,033 Views
macl
Senior Contributor I

The USB performance was improved in MQX 4.0.  Worthwhile to upgrade.

View solution in original post

0 Kudos
Reply
2 Replies
2,033 Views
praveenhegde
Contributor I

HI Amish, I am getting the same problem you faced. It takes around 80-90 seconds for copying the .bin file from a thumb drive. But I am already using MQX 4.0. I am new to the MQX. What could be the reason.

I am using fread() for reading a file from thumb drive. and I am working on K60 tower kit.

0 Kudos
Reply
2,034 Views
macl
Senior Contributor I

The USB performance was improved in MQX 4.0.  Worthwhile to upgrade.

0 Kudos
Reply