USB Error 0x10 and 0x0 with MQX USB MSD Disk example code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Error 0x10 and 0x0 with MQX USB MSD Disk example code

Jump to solution
2,465 Views
bobf
Contributor III

Hi Freescale Support,

 

The problem reported below probably indicates some kind of problems in USB device driver code. I hope someone in Freescale could take a look and fix it. The following are simple steps to reproduce it:

 

1) Compile PSP, BSP, MFS, RTCS, Shell, and USB libraries for kwikstik

 

2) Import and build unchanged example project MQX3_8\usb\device\examples\msd\disk\cw10\msd_disk_kwikstikk40x256 in CW 10.2. My build machine is running on Windows 7 32 bit.

 

3) Use menu Run | Debug Configurations to load and run it without any breaking point. Hit run icon to let it run if it breaks.

 

4) Connect the other USB port to a Windows 7 64 bit machine in order to use the newly created MSD disk.

 

Now every 1 or 2 minutes, the following 2 lines will be output in debug console in CW10.2:

 

USB Err: 0x10

USB Err: 0x0

 

with the 1st time (on plugging in) breaking at:

 

void

_mqx_idle_task

   (

     

/* [IN] parameter passed to the task when created */

     

uint_32 parameter

   )

{

/* Body */

  

volatileKERNEL_DATA_STRUCT _PTR_ kernel_data;

 

   _GET_KERNEL_DATA(kernel_data);  <---- break here

 

 

BTW, if choose Run | Run Configurations, it will end up with "terminated, exit code 0" quickly. Is this behavior normal? Does it suppose to run continously in some kind of loop instead of exiting?

 

Also can Freescale make this example to run in USB 2 high speed instead of full speed by default? It does not make sense to run at low speed when most USB ports are capable of high speed now. It'd be better to have a good and solid USB MSD example as a starting point for users like me.

 

Please take a look.

 

Thanks,

bobf

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,168 Views
bobf
Contributor III

Just found out this, but it's hard to believe: No USB high speed support for Kinetis in MQX up to this date, and many  Kinetis parts are not even capable of USB HS.

 

bobf

View solution in original post

0 Kudos
Reply
2 Replies
2,169 Views
bobf
Contributor III

Just found out this, but it's hard to believe: No USB high speed support for Kinetis in MQX up to this date, and many  Kinetis parts are not even capable of USB HS.

 

bobf

0 Kudos
Reply
2,168 Views
c0170
Senior Contributor III

Hi bobf,

 

MQX is going to support HS host. By the way, it's common mcu supports only FS, isn't it?

 

Regards,

MartinK

0 Kudos
Reply