USB Debug with TWR-K60N512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Debug with TWR-K60N512

Jump to solution
2,007 Views
davidcav
Contributor II

I am testing the Kinetis60 tower with the USB connector and the IAR Embedded Workbench IDE.  I have not been able to connect/debug/download code via the USB (OSBDM).  The drivers are installed on my computer but I get the following error message when I try to connect:

 

 

 "Fatal Error: Can not connect to J-Link via USB"

 

I attempted to try to configure the Project->Options->Debugger to other drivers, but was unsuccessful. 

 

Does anyone know the settings to allow the IAR to connect via USB?

0 Kudos
Reply
1 Solution
1,440 Views
DavidS
NXP Employee
NXP Employee

Hi Davidcav,

Some of the IAR projects default to using the JLINK JTAG debugger interface.  When Kinetis was first out and being tested that was the only debugger interface available.

Now the OSJTAG from P&E is used on the Tower.

Highlight your application project and select Options.

Then click onthe Debugger Category.

Set the Driver to PE micro.

Click OK.

Regards,

David

View solution in original post

0 Kudos
Reply
1 Reply
1,441 Views
DavidS
NXP Employee
NXP Employee

Hi Davidcav,

Some of the IAR projects default to using the JLINK JTAG debugger interface.  When Kinetis was first out and being tested that was the only debugger interface available.

Now the OSJTAG from P&E is used on the Tower.

Highlight your application project and select Options.

Then click onthe Debugger Category.

Set the Driver to PE micro.

Click OK.

Regards,

David

0 Kudos
Reply