USB CDC Virtual Com Example Not Working on TWR-K60N512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB CDC Virtual Com Example Not Working on TWR-K60N512

ソリューションへジャンプ
1,903件の閲覧回数
vwong
Contributor I

I am trying to use the CDC Virtual Com Example on TWR-K60N512 and  TWR-SER, with CW10.2 and MQX 3.8.

This is the cdc_vcom_twrk60n512 example project in the MQX 3.8 folder.

I can build and run in debug mode. But when I plug in a USB cable between the USB on TWR-SER board and the PC

USB, the PC does not see the USB device. Further debug it looks like the USB init task did not get executed by the RTOS and the RTOS is running in an idle loop task.

Is my problem the RTOS task structure no set up correctly?

 

Thanks,

VWong

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,559件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi VWong,

The MQX3.8.1 update seems to have the virtual comm example working.

Please update and test.  Alsom make sure you have most up-to-date "Terminal Untility" from www.pemicro.com with version 2.05 or newer.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,560件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi VWong,

The MQX3.8.1 update seems to have the virtual comm example working.

Please update and test.  Alsom make sure you have most up-to-date "Terminal Untility" from www.pemicro.com with version 2.05 or newer.

Regards,

David

0 件の賞賛
返信
1,559件の閲覧回数
Monica
Senior Contributor III

Hey Vincent! How is that going? Still having problems?

Tech guys are working on the issue, thank you very much for waiting up...if any news, you'll let us know please?

Regards!

Monica

0 件の賞賛
返信