USB CDC Virtual Com Example Not Working on TWR-K60N512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB CDC Virtual Com Example Not Working on TWR-K60N512

Jump to solution
1,359 Views
vwong
Contributor I

I am trying to use the CDC Virtual Com Example on TWR-K60N512 and  TWR-SER, with CW10.2 and MQX 3.8.

This is the cdc_vcom_twrk60n512 example project in the MQX 3.8 folder.

I can build and run in debug mode. But when I plug in a USB cable between the USB on TWR-SER board and the PC

USB, the PC does not see the USB device. Further debug it looks like the USB init task did not get executed by the RTOS and the RTOS is running in an idle loop task.

Is my problem the RTOS task structure no set up correctly?

 

Thanks,

VWong

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,015 Views
DavidS
NXP Employee
NXP Employee

Hi VWong,

The MQX3.8.1 update seems to have the virtual comm example working.

Please update and test.  Alsom make sure you have most up-to-date "Terminal Untility" from www.pemicro.com with version 2.05 or newer.

Regards,

David

View solution in original post

0 Kudos
Reply
2 Replies
1,016 Views
DavidS
NXP Employee
NXP Employee

Hi VWong,

The MQX3.8.1 update seems to have the virtual comm example working.

Please update and test.  Alsom make sure you have most up-to-date "Terminal Untility" from www.pemicro.com with version 2.05 or newer.

Regards,

David

0 Kudos
Reply
1,015 Views
Monica
Senior Contributor III

Hey Vincent! How is that going? Still having problems?

Tech guys are working on the issue, thank you very much for waiting up...if any news, you'll let us know please?

Regards!

Monica

0 Kudos
Reply