USB Bug?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Bug?

Jump to solution
2,381 Views
msinger
Contributor I

In host_dev_list.c on line 430  of MQX 3.7 is the call

 

  status = _usb_host_ch9_get_descriptor((pointer)new_instance_ptr,
      USB_DESC_TYPE_DEV << 8, 0, 8,  
      (uchar_ptr)&new_instance_ptr->dev_descriptor);
     


Should the "8" be an 18 as it's the length of the descriptor?

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,040 Views
c0170
Senior Contributor III

Hi msinger,

 

what you have found it's not bug. The device descriptor has size more than 8, according to specification. It is allowed to read only part of the descriptor.

 It is an intention to read just 8 Bytes of the descriptor.

 

Regards,

MartinK

View solution in original post

0 Kudos
Reply
2 Replies
2,041 Views
c0170
Senior Contributor III

Hi msinger,

 

what you have found it's not bug. The device descriptor has size more than 8, according to specification. It is allowed to read only part of the descriptor.

 It is an intention to read just 8 Bytes of the descriptor.

 

Regards,

MartinK

0 Kudos
Reply
2,040 Views
hchristo
Contributor I

did you solve this issue? i am trying to use the 3.6.1 usb stack in external ram (via mem_extend). the msd attaches, is supported, but the stack reports "unable to open USB disk".

 

the USB stack works ok for FAT-16 USB MSDs when run completely from internal ram.

0 Kudos
Reply