USB-Bluetooth Adapter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB-Bluetooth Adapter

ソリューションへジャンプ
2,748件の閲覧回数
Babak
Contributor I

Hi all,

 

i have the 52259 demo board, with codewarrior 7.1 and Freescale MQX 3.0. my task is to connect Wiimote to the board and i imagine one the solutions for this is the USB-Bluetooth adapter (the other might be using the Ethernet interface of the board but i'm still not sure how close Ethernet and bluetooth are and how difficult it is to do)

 

so for start i need some driver for connecting a USB-Bluetooth adapter to the board..as i've understood there is no support for this in the existing libraries though there might be support for low-level functions...

 

so any suggestions? anywhere i can find the driver i need? or should i go through writing the driver myself?!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,555件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hi Babak. Unfortunatelly, no such driver is written in MQX yet.

Message Edited by JuroV on 2010-02-08 09:45 AM

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,556件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hi Babak. Unfortunatelly, no such driver is written in MQX yet.

Message Edited by JuroV on 2010-02-08 09:45 AM
0 件の賞賛
返信