Two questions for MQX versions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two questions for MQX versions

ソリューションへジャンプ
1,399件の閲覧回数
huishao2
Contributor IV

1. Where can I find the version number of my MQX being  used?

2. After upgrading to MQX 4.1.1, the data type like uint_8 are all changed to something like uint8_t. Where is the proper place to resolve such backward compatibility issues?

Thanks!

Hui

タグ(4)
0 件の賞賛
返信
1 解決策
1,123件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

For the #2, check the Getting started guide :

3 Porting User Applications to MQX RTOS version 4.1.0

Starting with the MQX RTOS version 4.1.0, the standard C99 integer and boolean types (from stdlib.h and stdbool.h) are

used instead of the proprietary MQX types. When porting the application to the MQX RTOS version 4.1.0, compilation

issues could occur. The psptypes_legacy.h header file is available and contains the definition of the MQX legacy types. This

file can be included in the MQX application to overcome most of the compilation problems caused by the change of types.

To avoid potential problems, adopt the C99 types in your application.

For the #1 I use to check the release notes version in the installed folder. But perhaps there is other place to look at.

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,123件の閲覧回数
nitinharish
Contributor V

For #1:

See the "_mqx_version" string in here for e.g.:

C:\Freescale\Freescale_MQX_4_1\mqx\source\kernel\mqx.c

This will give you the exact build.

1,124件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

For the #2, check the Getting started guide :

3 Porting User Applications to MQX RTOS version 4.1.0

Starting with the MQX RTOS version 4.1.0, the standard C99 integer and boolean types (from stdlib.h and stdbool.h) are

used instead of the proprietary MQX types. When porting the application to the MQX RTOS version 4.1.0, compilation

issues could occur. The psptypes_legacy.h header file is available and contains the definition of the MQX legacy types. This

file can be included in the MQX application to overcome most of the compilation problems caused by the change of types.

To avoid potential problems, adopt the C99 types in your application.

For the #1 I use to check the release notes version in the installed folder. But perhaps there is other place to look at.

Luis

0 件の賞賛
返信