I am attempting to build the k60 tower demo using CW10.2 and MQX 3..8. The demo had paths to MQX 3.7 which I updated to 3.8. The demo compiles with 1 declaration systax error in CGI_index.c line 272
_mqx_int cgi_toggle_led4(HTTPD_SESSION_STRUCT *session)
{
  SetOutput(LED4,!GetOutput(LED4));
  return session->request.content_len;
}
Has anyone been through this? Is this something I caused or an issue with the update from MQX 3.7 to 3.8.?
Anyone get the tower K60 demo to compile in this configuration?
已解决! 转到解答。
Hello barber colman,
glad you solved your compile problem, regarding the warning, here's the thread which might shed some light on:
https://community.freescale.com/thread/97430
Regards,
MartinK
Hello,
could you be more precise? Which demo did cause the error ? What is located on the line 272? I would guess function/macro SetOutput..
Some demos might have been updated because of using a lwgpio driver.
Regards,
MartinK
 
					
				
		
I am using a downloaded copy of of the TWR-K60N512_Quick_Start_Demo. The error is at line 272 file cgi_index.c. The code I posted is the code located at line 272 of file cgi_index.c.
For some reason the compiler does not like _mqx_int cgi_toggle_led4 and I do not see why.
_mqx_int cgi_toggle_led4(HTTPD_SESSION_STRUCT *session)
{
  SetOutput(LED4,!GetOutput(LED4));
  return session->request.content_len;
}
 
 
					
				
		
I was looking at the code and saw no reason for the error so I reinstalled the demo and it now compiles. No idea what happended.
I am now getting warningsbut it compiles. I have pasted a copy of one of the warnings below. Anyone know why a demo is getting this warning and can I ignore them?
Thankse
Symbol device_array multiply defined in usb_ddk_twrk60n512_d.a(usb_hid.o ) and usb_ddk_twrk60n512_d.a(usb_audio.o ) Ignoring the definition in usb_ddk_twrk60n512_d.a(usb_hid.o ) TWR-K60N512_Quick_Start_Demo C/C++ Problem
Hello barber colman,
glad you solved your compile problem, regarding the warning, here's the thread which might shed some light on:
https://community.freescale.com/thread/97430
Regards,
MartinK