Token not expected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Token not expected

1,603 Views
Teckna
Contributor V

Hi everyone,

I'm not sure if this is the correct section where I have to show my problem: if so, please move the topic in the correct section.

I'm using MQX 4.1 and CW 10.2.
I'm trying to build the bsp_twrmcf52259 project, but no matter which file is compiling, I receive always the same error:
- Token 'equals' not expected

If I use the CW 10.6 (evaluation with eval period terminated) everything is ok.

Is there some incompatibility between MQX 4.1 and CW 10.2 or is there some settings to do?

Many thanks
Teckna

0 Kudos
Reply
2 Replies

1,506 Views
Teckna
Contributor V

Just another question: is there someone that knows where I can find the 'equals' token? I searched in source and project files but with no result.

Many thanks

Teckna

0 Kudos
Reply

1,506 Views
soledad
NXP Employee
NXP Employee

Hi Teckna,

Freescale MQX RTOS was compiled and tested with CodeWarrior Development Studio for Microcontrollers version 10.6. So, I suggest you to install CW10.6.

You can download it from the next link:

CodeWarrior for MCUs (Eclipse IDE) - ColdFire|Freescale


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------