Timer Interrupts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Timer Interrupts

Jump to solution
4,505 Views
Awera
Contributor III

Hi

 

How can I use a DTIM interrupt?

 

I want to create a periodic interrupt but I don't know how. I have used the ISR example of MQX's folder but I don't want to use PIT for my service.

 

Has anyone an example?

 

Thank you

0 Kudos
Reply
1 Solution
3,367 Views
LordMark
Contributor IV

I'm using M52259DEMOKIT.

 

I'm using GPT for output compare match with the following code:

 

 

VMCF5225_STRUCT_PTR  reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR;[...]void gpt_init (){ reg_ptr -> GPT.GPTIOS |= GPT_GPTIOS_IOS0;     //Attivazione Output Compare 0   reg_ptr -> GPT.GPTC0 = 0x00;        //GPTC0 resettato a 0   reg_ptr -> GPT.GPTDDR |= GPT_GPTDDR_DDRT0;     //Pin OC0 come uscita    reg_ptr -> GPT.GPTCTL1 |= GPT_GPTCTL1_OUTPUT0_NOTHING;  //Nessun effetto sul piedino OC0    reg_ptr -> GPT.GPTSCR2 |= GPT_GPTSCR2_PR_16;    //Prescaler 1/16      _int_install_kernel_isr (MCF5225_INT_TIMA_C0F, OC0_service);        reg_ptr -> GPT.GPTFLG1 |= GPT_GPTFLG1_CF0;     //clear flag   reg_ptr -> GPT.GPTIE |= GPT_GPTIE_CI0;      //Interrupt su OC0       _mcf5225_int_init (MCF5225_INT_TIMA_C0F, gpt_level, gpt_priority, 1);}[...]__declspec(interrupt:0) void OC0_service (){    count++;    reg_ptr -> GPT.GPTFLG1 |= GPT_GPTFLG1_CF0;     //clear flag}

 

I set MQX_ROM_VECTORS to 0 in the user_config.h and rebuilt bsp and psp. In the code I'm using the function _int_install_kernel_isr so that my interrupt routine is direct without MQX intervention. (It should allow faster interrupts)

 

You may try to modify the code to your purposes. Hope it helps.

 

Moreover, something about the DTIM is here https://community.freescale.com/message/60070#60070

 

Regards,

Marco

 

 

View solution in original post

0 Kudos
Reply
4 Replies
3,368 Views
LordMark
Contributor IV

I'm using M52259DEMOKIT.

 

I'm using GPT for output compare match with the following code:

 

 

VMCF5225_STRUCT_PTR  reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR;[...]void gpt_init (){ reg_ptr -> GPT.GPTIOS |= GPT_GPTIOS_IOS0;     //Attivazione Output Compare 0   reg_ptr -> GPT.GPTC0 = 0x00;        //GPTC0 resettato a 0   reg_ptr -> GPT.GPTDDR |= GPT_GPTDDR_DDRT0;     //Pin OC0 come uscita    reg_ptr -> GPT.GPTCTL1 |= GPT_GPTCTL1_OUTPUT0_NOTHING;  //Nessun effetto sul piedino OC0    reg_ptr -> GPT.GPTSCR2 |= GPT_GPTSCR2_PR_16;    //Prescaler 1/16      _int_install_kernel_isr (MCF5225_INT_TIMA_C0F, OC0_service);        reg_ptr -> GPT.GPTFLG1 |= GPT_GPTFLG1_CF0;     //clear flag   reg_ptr -> GPT.GPTIE |= GPT_GPTIE_CI0;      //Interrupt su OC0       _mcf5225_int_init (MCF5225_INT_TIMA_C0F, gpt_level, gpt_priority, 1);}[...]__declspec(interrupt:0) void OC0_service (){    count++;    reg_ptr -> GPT.GPTFLG1 |= GPT_GPTFLG1_CF0;     //clear flag}

 

I set MQX_ROM_VECTORS to 0 in the user_config.h and rebuilt bsp and psp. In the code I'm using the function _int_install_kernel_isr so that my interrupt routine is direct without MQX intervention. (It should allow faster interrupts)

 

You may try to modify the code to your purposes. Hope it helps.

 

Moreover, something about the DTIM is here https://community.freescale.com/message/60070#60070

 

Regards,

Marco

 

 

0 Kudos
Reply
3,367 Views
Awera
Contributor III

Thank you very mauch Marco

 

I have a question about timer PIT0: if I change the PIT0's registers in my main task, the functions like _time_add or _time_get and others, will be change? I mean if I can use this functions in the same way than before changing this registers.

 

Thanks

0 Kudos
Reply
3,367 Views
LordMark
Contributor IV

Well, I never used PIT timer so I cannot answe you precisely. But I think that you can use those function anyway. They only involve ticks and no other settings.

3,367 Views
Awera
Contributor III

Thank you Mark.

 

Your posts has been really useful for me

0 Kudos
Reply