Timeline view doesn't work in example and LOG_OVERWRITE crashes CW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Timeline view doesn't work in example and LOG_OVERWRITE crashes CW

914 Views
OldPeculier
Contributor II

Hi all,

I'm testing timeline view with the example klog.c.  When I try to view, I get "No task switches found" and yet _klog_create returns MQX_OK, and _klog_control is set to the example default.  Moreover, MQX Log Summary view is showing 170 log entries under kernel logging.

Ironically it works in my application if _klog_create switch = 0.  The reason I am attempting the example is that if I set switch = LOG_OVERWRITE in my application, CW 3.8 crashes so hard I have to reboot the computer (W7).

Thanks for any help

Martin

0 Kudos
Reply
1 Reply

812 Views
trytohelp
NXP Employee
NXP Employee

Hi  Martin,

You're using MQX lib.

What is the CodeWarrior version used ?

What is the processor and do you use a project example ?

      Which one ?

Regards

Pascal

0 Kudos
Reply