The bootloader with SD card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The bootloader with SD card

1,420 次查看
小勇邹
Contributor II

There are two parts in my application- the bootloader part(without MQX OS)  +  the user application part(with MQX OS).

The SD card is used in my application. The new firmware is stored in the SD card.

The bootloader should get the new firmware from the SD card and copy it to the MCU.

If the bootloader does not support MQX system, is it possible to access the firmare in SD card by file address?

For example,the firmware is put in the address \Firmware\BasicUnit in the SD card.

The bootloader without MQX OS  want to get the firmware from the address in the SD card.

How should I do? Is there any example to do that?

The hardware is K64 and the OS is Freescale_MQX_4_1_TWRK64F120M.

0 项奖励
回复
2 回复数

1,244 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Robin:

We have a bootloader based on USB stack, it uses the FAT file system-supporting module to read an image file and then uses the bootloader driver to program the image file to the flash memory of the device. So it is possible to access the image file in USB stick.

pastedImage_0.png

For details, please refer to the document

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4368.pdf

You also can download the associated source code AN4368 from Freescale website.  The demo is based on K60, not K64

For SD card support, we do not have an existing demo, I think you need to add sd card support into this bootloader package.

Have a nice day,
Daniel

0 项奖励
回复

1,244 次查看
小勇邹
Contributor II

Dear Daniel,

Thank you very much for your help.

Does the SD card example in C:\Freescale\MQX_KSDK_1.0.0\demos\sdhc_sdcard\iar\twrk64f120m work without MQX? 

I think there are two solutions for me.

Solution 1:

Let the boot loader work without MFS.

Is it possible to put the firmware to specific address (for example:0xffff000) in the SD card by the user application with MQX OS and get the firmware from specific address(for example:0xffff000)  in the SD card by the boot loader without MQX OS? I just want to get the firmware from the SD card in
specific address and do not care about the file address or file format.

Solution 2:

Let the boot loader work with  MFS.

I want to modify the source code based on the example C:\Freescale\MQX_KSDK_1.0.0\demos\sdhc_sdcard\iar\twrk64f120m.
Is it possible to add the mfs module to the example?

Best regards.

Robin Zou.

0 项奖励
回复