The AN3906 application which is serial to ethernet bridge , and the source code is available with free RTOS , is there source code for the serial to ethernet bridge using Freescale MQX on K60 tower

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The AN3906 application which is serial to ethernet bridge , and the source code is available with free RTOS , is there source code for the serial to ethernet bridge using Freescale MQX on K60 tower

1,432 Views
vallinaths
Contributor II

having K60 tower with TWR SER need  source code to check the serial to Ethernet bridge conversion for one of the application , is it available if so please chare it

Labels (1)
0 Kudos
Reply
2 Replies

1,075 Views
karelm_
Contributor IV

Hi,

there will be new Ethernet to serial demo in the MQX 4.0.2. This version is not released yet, but I can give you source code of this demo (it is in attached zip). It should work on all platforms (including K60). There is also readme PDF which you can use as guide for setting this application up.

Best regards

Karel Mozny

1,075 Views
vallinaths
Contributor II

Hi karel,

thanks for sharing the code will check

0 Kudos
Reply