Task Suspension

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,050件の閲覧回数
netra
Contributor IV

I am using mqx 3.5 (MCF52259),

I want to suspend a thread using shell command .

Can anyone tell me how to do??

1 解決策
1,739件の閲覧回数
Martin_
NXP Employee
NXP Employee

https://community.freescale.com/message/329949#329949

for example, set an event or semaphore. the task would poll the event/semaphore in a while(1) loop and call _task_block() in response to it.  alternatively you can use task queue to suspend/resume tasks (_taskq_suspend_task(), _taskq_resume()).

元の投稿で解決策を見る

2 返答(返信)
1,740件の閲覧回数
Martin_
NXP Employee
NXP Employee

https://community.freescale.com/message/329949#329949

for example, set an event or semaphore. the task would poll the event/semaphore in a while(1) loop and call _task_block() in response to it.  alternatively you can use task queue to suspend/resume tasks (_taskq_suspend_task(), _taskq_resume()).

1,739件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Netra,

Wow that is very old version of MQX.  Please note latest download (http://www.freescale.com/mqx) is MQX4.0.2.GA.

In your MQX3.5\docs\mqx\MQXUG.pdf please review information on the following:

2.6.7 Task Queues

In addition to providing a scheduling mechanism, task queues provide a simple and efficient way to

synchronize tasks. You can suspend tasks in the task queue and remove them from the task queue.

Regards,

David