TWR_K20D72M MQX Lite PE USB stack problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR_K20D72M MQX Lite PE USB stack problem

ソリューションへジャンプ
2,028件の閲覧回数
marcbunyard
Contributor IV

I am working on the TWR_K20D72M using PE with MQX Lite and the USB_LDD, and it won't enumerate.  I have used the example in C:\Freescale\CW MCU v10.4\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K20D72M\USB_MS_Device, and seems to set everything up correctly, but when the Host performs GetDeviceDescriptor, erroneous data in sent in response to the IN packet.  The example does not use MQX Lite, and when I run it as is, it works.

I can't find an example of MQX Lite with PE and USB for the K20.  Is there one?

タグ(5)
0 件の賞賛
返信
1 解決策
1,742件の閲覧回数
marcbunyard
Contributor IV

I moved the DeviceDescriptor data from ROM to RAM, and the data problem has cleaned up. 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,743件の閲覧回数
marcbunyard
Contributor IV

I moved the DeviceDescriptor data from ROM to RAM, and the data problem has cleaned up. 

0 件の賞賛
返信
1,742件の閲覧回数
Monica
Senior Contributor III

Marc,

that is great, thank you very much for sharing your resolution! :smileygrin:

Best regards,

Monica

0 件の賞賛
返信