TWR_K20D72M MQX Lite PE USB stack problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR_K20D72M MQX Lite PE USB stack problem

跳至解决方案
2,106 次查看
marcbunyard
Contributor IV

I am working on the TWR_K20D72M using PE with MQX Lite and the USB_LDD, and it won't enumerate.  I have used the example in C:\Freescale\CW MCU v10.4\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K20D72M\USB_MS_Device, and seems to set everything up correctly, but when the Host performs GetDeviceDescriptor, erroneous data in sent in response to the IN packet.  The example does not use MQX Lite, and when I run it as is, it works.

I can't find an example of MQX Lite with PE and USB for the K20.  Is there one?

标记 (5)
0 项奖励
回复
1 解答
1,820 次查看
marcbunyard
Contributor IV

I moved the DeviceDescriptor data from ROM to RAM, and the data problem has cleaned up. 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,821 次查看
marcbunyard
Contributor IV

I moved the DeviceDescriptor data from ROM to RAM, and the data problem has cleaned up. 

0 项奖励
回复
1,820 次查看
Monica
Senior Contributor III

Marc,

that is great, thank you very much for sharing your resolution! :smileygrin:

Best regards,

Monica

0 项奖励
回复