TFTP Client "PUT" operation?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TFTP Client "PUT" operation?

1,057件の閲覧回数
cwpaynter
Contributor III

I'm running MQX 4.01, looking at the RTCS demo project, specifically the TFTP client, running on a TWR-K60N512.  As far as I can see, it only supports reading a file from a remote server, not writing one to the server.  Anybody ever find a way to do this?

The shell command Shell_TFTP_client() in sh_tftp.c has a comment in the function header which hints that it will "TFTP to or from a host", but I don'd see any way to do it from there.  tftp.c seems only to support "get" operations with function TFTP_read().

thanks!

Chris

タグ(4)
0 件の賞賛
返信
0 返答(返信)