Size of the application has exceeded the capability of this license. Contact your authorized distributor or Freescale to purchase a full version of the tools. USBK60

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Size of the application has exceeded the capability of this license. Contact your authorized distributor or Freescale to purchase a full version of the tools. USBK60

1,625 次查看
anjalishyju
Contributor III

Dear all,

I am working on USB host development using MQX RTOS.I am trying to implement example code from MQX (Path: Freescale_MQX_4_0\mfs\examples\mfs_usb\cw10\mfs_usb_twrk60f120m).

It needs packages such as bsp, psp, shell, mfs & usbhost. Downloaded and installed the Codewarrior10.5 on 3 days ago. When compiling the sample code it shows the error such as " Size of the application has exceeded the capability of this license. Contact your authorized distributor or Freescale to purchase a full version of the tools".

Please help me.

0 项奖励
回复
2 回复数

1,247 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

I wonder you should use special edition CW that has 128k c code size limitation.

in CW10.5, all version(special standard professional ) can support MQX for kinetis.(in older version, only professional edition can support MQX for kinetis) but because special edition has very limit code size limitation and MQX  project normally big size, we suggest user use standard or professional edition CW.

you can download CW10.5 evaluation edition to test your MQX project . here is CW10.5 evaluation download link

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=015210272600612247

or

you can write to support@freescale.com to request a CW10.5 evaluation license

0 项奖励
回复

1,247 次查看
soledad
NXP Employee
NXP Employee

Hi Anjali


This error is caused by the license. Please be sure that you have installed  CodeWarrior™ Professional Edition.

Regards

Sol

0 项奖励
回复