Simple RTC causing unhandled interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simple RTC causing unhandled interrupt

Jump to solution
1,928 Views
LordMarkFRT
Contributor II

Hi everyody. I'm using MCF52259demokit and MQX 3.6. I'm fightint against the main task that after 2 or 3 hours of running (or debugging) launches an unhandled interrupt. The only peripheral I'm using is the RTC with 1Hz interrupt. So I think that RTC must be the cause of the issue.

 

I'm attaching the code for anyone who wants to try it, or take a look at it to see if there is something wrong. 

 

Regards,

Marco

0 Kudos
Reply
1 Solution
1,661 Views
LordMarkFRT
Contributor II

SEEMS solved by porting it to MQX 3.7.

View solution in original post

0 Kudos
Reply
1 Reply
1,662 Views
LordMarkFRT
Contributor II

SEEMS solved by porting it to MQX 3.7.

0 Kudos
Reply