Serial interrupt mode: ttyb vs ittyb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Serial interrupt mode: ttyb vs ittyb

ソリューションへジャンプ
1,949件の閲覧回数
Ardoster
Contributor III

Hi

 

After some time without using MQX, i have received a new project using MQX, so here I am. :smileyhappy:

 

I've been reading about using the serial port in interrupt and polling mode. So: using ttyb for polling mode, and using ittyb for interrupt mode. But the example project (mqx\examples\io) works correctly using ttyb either ittyb. So, my question is: MQX does something different internally? Or must I do a different code in my application to use ittyb as interrupt mode? For example, using _int_install_isr...???

 

Thanks for your help

 

Regards

 

 

 

0 件の賞賛
返信
1 解決策
1,383件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Ardoster,

Please review this previous post and if you have further questions we're happy to help.

https://community.freescale.com/thread/92638

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,384件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Ardoster,

Please review this previous post and if you have further questions we're happy to help.

https://community.freescale.com/thread/92638

Regards,

David

0 件の賞賛
返信