SSH for MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,144件の閲覧回数
ARQuattr
Contributor III

I am using MQX and would like to add SSH capability.  I have a couple of questions:

1. Where can I find information on the EAI SSH component including the cost and how to purchase this?  Does it include a client and server?  

2. Do either of the Mocana NanoSSH or Embedded Access SSH products allow reverse SSH tunneling (like the '-R' option in ssh)?

Thanks,
Angelo

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,545件の閲覧回数
rav
Contributor III

For the Freescale NanoSSL and NanoSSH, reverse SSH tunneling (like the '-R' option in ssh) is a feature requirement for the next release. 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,545件の閲覧回数
Nouchi
Senior Contributor II

Hello,

 

Freescale now provide Nano SSH client (Only) and Nano SSL, both can be bought from website.

0 件の賞賛
返信
2,545件の閲覧回数
ARQuattr
Contributor III

Does this mean they are not supporting the Embedded Access version ?

 

Has anyone used either of these packages?

0 件の賞賛
返信
2,546件の閲覧回数
rav
Contributor III

For the Freescale NanoSSL and NanoSSH, reverse SSH tunneling (like the '-R' option in ssh) is a feature requirement for the next release. 

0 件の賞賛
返信