SSH for MQX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SSH for MQX

Jump to solution
4,122 Views
ARQuattr
Contributor IV

I am using MQX and would like to add SSH capability.  I have a couple of questions:

1. Where can I find information on the EAI SSH component including the cost and how to purchase this?  Does it include a client and server?  

2. Do either of the Mocana NanoSSH or Embedded Access SSH products allow reverse SSH tunneling (like the '-R' option in ssh)?

Thanks,
Angelo

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,523 Views
rav
Contributor III

For the Freescale NanoSSL and NanoSSH, reverse SSH tunneling (like the '-R' option in ssh) is a feature requirement for the next release. 

View solution in original post

0 Kudos
Reply
3 Replies
2,523 Views
Nouchi
Senior Contributor II

Hello,

 

Freescale now provide Nano SSH client (Only) and Nano SSL, both can be bought from website.

0 Kudos
Reply
2,523 Views
ARQuattr
Contributor IV

Does this mean they are not supporting the Embedded Access version ?

 

Has anyone used either of these packages?

0 Kudos
Reply
2,524 Views
rav
Contributor III

For the Freescale NanoSSL and NanoSSH, reverse SSH tunneling (like the '-R' option in ssh) is a feature requirement for the next release. 

0 Kudos
Reply