SSH for MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SSH for MQX

跳至解决方案
4,121 次查看
ARQuattr
Contributor IV

I am using MQX and would like to add SSH capability.  I have a couple of questions:

1. Where can I find information on the EAI SSH component including the cost and how to purchase this?  Does it include a client and server?  

2. Do either of the Mocana NanoSSH or Embedded Access SSH products allow reverse SSH tunneling (like the '-R' option in ssh)?

Thanks,
Angelo

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,522 次查看
rav
Contributor III

For the Freescale NanoSSL and NanoSSH, reverse SSH tunneling (like the '-R' option in ssh) is a feature requirement for the next release. 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,522 次查看
Nouchi
Senior Contributor II

Hello,

 

Freescale now provide Nano SSH client (Only) and Nano SSL, both can be bought from website.

0 项奖励
回复
2,522 次查看
ARQuattr
Contributor IV

Does this mean they are not supporting the Embedded Access version ?

 

Has anyone used either of these packages?

0 项奖励
回复
2,523 次查看
rav
Contributor III

For the Freescale NanoSSL and NanoSSH, reverse SSH tunneling (like the '-R' option in ssh) is a feature requirement for the next release. 

0 项奖励
回复