SPI MQX set delays

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,020件の閲覧回数
cwati
Contributor III

Hi there,

I've been trying to port some SPI code from basic KSDK 1.0.0 to MQX 4.1 (SPI not SPI legacy).

Code works smoothly in KSDK 1.0.0, but I notice some timing issues in MQX 4.1.

We use the following set delays in KSDK.  Is there similar set delay functionality in MQX for SPI?

  status = DSPI_DRV_MasterSetDelay(instance,

    kDspiPcsToSck,

    500, // delayInNanoSec

    & calculatedPcsToSck);

  if (status != kStatus_DSPI_Success)

  return false;

    status = DSPI_DRV_MasterSetDelay(instance,

    kDspiLastSckToPcs,

    500, // delayInNanoSec

    & calculatedLastSckToPcs);

  if (status != kStatus_DSPI_Success)

  return false;

  status = DSPI_DRV_MasterSetDelay(instance,

    kDspiAfterTransfer,

    500, // delayInNanoSec

    & calculatedAfterTransfer);

  if (status != kStatus_DSPI_Success)

  return false;

Thanks,
Cecylia

タグ(4)
0 件の賞賛
返信
1 解決策
1,760件の閲覧回数
cwati
Contributor III

Hmmmpf, doesn't seem like MQX has explicit IOCTLs to set delays (KSDK "DSPI_DRV_MasterSetDelay") but if you set the baud rate correctly, MQX' "_dspi_find_baudrate" will resolve it for you.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,761件の閲覧回数
cwati
Contributor III

Hmmmpf, doesn't seem like MQX has explicit IOCTLs to set delays (KSDK "DSPI_DRV_MasterSetDelay") but if you set the baud rate correctly, MQX' "_dspi_find_baudrate" will resolve it for you.

0 件の賞賛
返信
1,760件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

I think in mqx, you can use wait function, but the resolution is not fine. Thank you for your sharing.

0 件の賞賛
返信