SCI High speed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCI High speed

2,206件の閲覧回数
oscar
Contributor I

I'm trying to communicate at serial high speed (460800 bps and 921600 bps) but I received wrong characters.

 

My design:

- I'm using the serial MQX driver (3.7) in interrupt mode and I configured it for this speed (other speeds works well). 

- I'm using a 48MHz crystal.  

 

I read that it's possible to use (the baudrate register supports it).

Any idea about this topic?

 

Thanks in advance.

0 件の賞賛
返信
4 返答(返信)

2,055件の閲覧回数
GottiLuca
Contributor IV

Dear Oscar,

 

I have had same issues with MQX 3.7 with TWRK60 BSP . Follow this link for the details and a possible solution :

 

https://community.freescale.com/thread/87446

 

2,055件の閲覧回数
oscar
Contributor I

First, thanks for your quick response.

I saw your suggestion but I'm using the  MCF52259 and it doesn't has a Baud Rate Fine Adjust (BRFA) register or similar....

0 件の賞賛
返信

2,055件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Oscar,

It's been awhile since I ran a test to see how fast the UART can run on ColdFire but what I recall is that the raw UART signal was fine but the UART transceiver has a lower max frequency capability.  I think I used oscope on input and output of transceiver to see the signal integrity to determine what was the system max frequency/baud I could use.

Hope this helps.

Regards,

David

 

2,055件の閲覧回数
oscar
Contributor I

It's a communication between 2 microcontrollers ( no transceivers used) . The problem is: High %error transmission when when using the internal clock source...I'm thinking to use a external clock source...

0 件の賞賛
返信